Gadget Renesas

Linking Ideas and Electronics

Item

GR-CITRUS Special Project

Starting out with Rubic (Ruby version)

Overview

GR-CITRUS can be run using the Ruby language. This article describes how to program using the Chrome app Rubic with Windows or MAC.

Preparation

Hardware

You will need a GR-CITRUS board and a USB cable (micro B type).

login login


Software

Install Rubic by opening the Rubic page on the Chrome website and adding the Rubic app to your browser. If you don’t have the Chrome web browser installed on your computer, you will need to do this first.

login


PC connection and USB driver

Connect the GR-CITRUS board to your PC. Your PC may need to recognize the USB driver, so you will need to download and specify the following ini file.

Click the link below to start the download. After the download is complete, decompress the file.

GR_CITRUS_USBCDC.zip

When the board is successfully connected to your PC, the red LED will light up. If it doesn’t, this may indicate that there is no RUBY firmware programmed to GR-CITRUS. In this case, please refer to the site link below titled “Recovering Ruby firmware.”

login

 

Protocol

1. Startup Rubic

Open the Chrome browser and click Sketch in the browser tool bar. In the displayed app list, click Rubic to start the application.

login



2. Specify the board and port

Specify the following from the pull-down menu to the lower left of the Rubic screen.
Hardware configuration: GR-CITRUS
Connection destination; COM** (Windows)、/dev/tty.usbmodem1.1 (Mac)

(Set using the buttons on the lower left circled in red.)

login


(Select GR-CITRUS under Board Type.)

login


(Set the firmware and revision with the board function tab.)

login


Press the Information button to display version information. This display indicates that the state is ready for Rubic and GR-CITRUS to communicate successfully.

login



3. Run the program

So, let’s try executing a simple program. Copy the following program to Rubic and press the Run button. The LED on GR-CITRUS should flash.
After this, repeated create and run programs.

10.times do
    led 1
    delay 100
    led 0
    delay 100
end
     

login



 

Sample

Refer to the github link below for Ruby samples programmed for GR-CITRUS.
github.com/wakayamarb/wrbb-v2lib-firm/tree/master/sample/GR-CITRUS

Supply power, then execute the Ruby program

The GR-CITRUS board is set (default state) to wait for communication with Rubic. After supplying power to the board by shorting the START jumper as circled in red below, the MCU will automatically run the Ruby program written to GR-CITRUS.

login

Ruby firmware recovery

It is a link to GR-CITRUS's latest firmware for Ruby. To write the firmware, please press the reset button of GR-CITRUS and recognize it as USB memory, then copy the bin file. About the latest firmware, refer to Github.

GR-CITRUS Ruby firmware V2.35

citrus_mruby_V235.bin

share