Gadget Renesas

Linking Ideas and Electronics

Item

IDE for GR

IDE for GR is the development environment that enables to program offline. You can use like Arduino IDE and import a sample, compile, write a program and debug via serial monitor.
* The current version is tentative. The following GR boards are supported
GR-SAKURA, GR-KAEDE, GR-KURUMI, GR-COTTON, GR-CITRUS, GR-PEACH, GR-ADZUKI and GR-LYCHEE

IDE for GR

Download

Click the following link to download.


V1.03

IDE for GR 1.03 (334MB, for Windows)

IDE for GR 1.03 (353MB, for Mac)


Update information:

  • Updated Feb 2nd, 2018 for windows. Feb 8th for mac.
  • Line numbers can now be displayed.
  • Ensure that "core dependency" error does not appear in Arduino library import.
  • Updated the library of GR-PEACH to V2.03. Addition of LCD libraries was done.
  • Updated the library of GR-LYCHEE to V1.02. Addition of LCD libraries was done.


V1.02

IDE for GR 1.02b (337MB, for Windows)

IDE for GR 1.02 (410MB, for Mac)


Note: The volume label of GR-CITRUS has been changed to "GR-CITRUS_b" by updating USB mass storage firmware. With V 1.02 or less, "GR-CITRUS is not found" is displayed at the time of writing. The Windows version is compatible with V1.02b. The Mac version will be compatible with V1.03 planned for December 2017. (Nov 8th 2017)


V1.01

IDE for GR 1.01 (322MB, for Windows)

IDE for GR 1.01 (393MB, for Mac)


V1.00

IDE for GR 1.00 (321MB, for Windows)

IDE for GR 1.00 (325MB, for Mac)

Notes

•About installation

For Windows, it is not in the installation format. After extracting the zip file, please start the exe file.
For Mac, after mounting the dmg file, move the IDE for GR to the application folder.

Supporting PC

Windows

- Windows 7 32/64bit
- Windows 8.1 32/64bit
- Windows 10 32/64bit

Mac

- OS X 10.9 Mavericks
- OS X 10.10 Yosemite
- OS X 10.11 El Capitan
- OS X 10.12 Sierra (Evaluated on V1.03)
- OS X 10.13 High Sierra (Evaluated on V1.03)


Technical Support

Technical Information
Related Web Site

Twitter

share